AXIS#.SM.MODE
Description
AXIS#.SM.MODE defines the mode of service motion for each loop. Two types of service motion are available :
- A constant motion in one direction (endless or for a certain amount of time).
- An alternating motion.
The possible modes for this parameter are described in the following table:
|
AXIS#.SM.MODE |
Description |
Requirements |
|---|---|---|
|
0 |
Constant motion in closed current loop mode of operation.
The service motion can be stopped by using the AXIS#.STOP command. |
AXIS#.OPMODE = 0,1, or 2 AXIS#.CMDSOURCE = 0 |
|
1 |
|
AXIS#.OPMODE = 0, 1, or 2 AXIS#.CMDSOURCE = 0
|
| 2 | This mode executes the same service motion as mode 0. However, the motion is described by AXIS#.SM.I2, AXIS#.SM.T2 and AXIS#.SM.V2. This enables a change on the fly and is mostly used under fieldbus control. |
AXIS#.OPMODE = 0, 1, or 2 AXIS#.CMDSOURCE = 0 |
Profiles
Service Motion for AXIS#.SM.MODE 0 and AXIS#.OPMODE 0 (Current)
Profile when AXIS#.SM.T1 is greater than 0:
Profile when AXIS#.SM.T1 equals 0:
Service Motion for AXIS#.SM.MODE 0 and AXIS#.OPMODE 1 or 2 (Velocity or Position)
Profile when AXIS#.SM.T1 is greater than 0:
Profile when AXIS#.SM.T1 equals 0:
Service Motion for AXIS#.SM.MODE 1 and AXIS#.OPMODE 0 (Current)
Service Motion for AXIS#.SM.MODE 1 and AXIS#.OPMODE 1 or 2 (Velocity or Position)
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.SM.MODE | 0x500E | 0x3 | UINT | - | - | RW | False |
| AXIS2.SM.MODE | 0x510E | 0x3 | UINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|